This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22916: Does the switch need input and output capacitors for very low current use ?

Part Number: TPS22916

Hello,

Does the TPS22916BYFP switch need input or output capacitors when using it in a very low current application (<15µA) ?

Vin is between 1.8V and 3.3V.

Thank you very much.

Regards,

Victor Tolosana