Hi Experts,
Could I ask whether LM5177 can meet Vout (5-48V). Iout (5A), Pout (240W) requirements, and Vin can be DC with voltage range not been restricted? Output power rating will be 5V/3A, 9V/3A, 15V/3A, 20V/3A, 20V/5A, 28V/5A, 36V/5A,and 48V/5A to meet PD3.1 Spec requirements. Also, if possible, could you help share how to identify the output voltage range with different current rating for a DCDC?
Thanks!
Dylan