Part Number: TPS62180
Hi team,
I tested TPS62180 and got two questions.
First question: When I use only one phase and run in light load, I can see the other phase switching in a certain frequency, which is about 110kHz. The picture is below, the green line is normal phase, the yellow line is 110kHz phase. Why does the second phase run in 110kHz?

Second question: When it runs in 2A, the switching frequency is 1.5MHz and phase differences is 90 degree. When it runs in 3A, the switching frequency is 2MHz and phase differences is 180 degree. The pictures are below. What does it cause the switching frequency and phase difference?


The circuit is below.

Best Regards,
Peter