This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25723: BQ25723 add system switch

Part Number: BQ25723


Hi

The customer design requirement as below:

Vin  15v, Iin max 10A ,       Vcharge:3 cell   Icharge  10-12A, 

They want to add a switch between system side. After pressing the switch, BQ25723 can enter the low power consumption mode, and Isys is limited to the uA pole;

Press the switch to the high level again to turn on Vsys power. It is applicable to both adapters and batteries.

It seems BQ25723 is not suitable.

Please recommend the chip that supports hardware switch setting of low power mode and performance mode(the function is similar to the power on key function of a laptop)

Waiting for your reply.

Thanks

Star