Part Number: TPS650860EVM-116
Other Parts Discussed in Thread: TPS650864
Hi
We are testing the TPS650860EVM-116 IRQB pin function. Below is my test step:
- Wire a 2.2 ohm on Buck6 output and GND connector.
- Change the R48 of the TPS650860EVM-116 component from 12.1K ohm to 330ohm. according to the formula of the datasheet of the SWCS142 my threshold should approach 0.188A. ("Rlim" can adjust the overcurrent threshold, and my max value of RDSON is 8.4mohm, ignore the Iripple.)
- Program TPS650860EVM-116 Buck6 output voltage in 1.5V, and thrn on the CNTL pin.
- Output current should approach 0.681A, then IRQB pin active.
According to the datasheet of the TPS650864, IRQB should be active when Buck1、2、6 power fault or overcurrent, But it's can't work.

I have a few quation below:
- Is my experiment correct, if I am not setting it wrong?
- Did I have another approach to test IRQB pin?