This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1: BQ40Z50R1

Part Number: BQ40Z50-R1
Other Parts Discussed in Thread: BQ40Z50

Hi

I have couple of question to be clarified which is listed below

1.We are using BQ40Z50-R1 IC. We have extracted the golden file and we are using in  production. Unfortunately the BQ40Z50-r1 is out of stock. For this we can use this BQ40Z50RSMT IC and we can upload the golden file.

2.In some battery lots during production we have used BQ40Z50SMT.During the upload of gas gauge file the following error occured, which is shown below

Error: The Data flash checksum calculated from srec does not match checksum returned from device after programming. 

Expecting your reply at the earliest.

Regards

MAX

  • Hello Max

    Does it succeed when you try again? If yes, then that would indicate noise on SMBus as the cause.

    Also check that the device is correctly powered during programming

  • Hi Shirish

    Thanks for the update

    We will check on it

    We have another one question shown below

    1.We are using BQ40Z50-R1 IC. We have extracted the golden file and we are using in  production. Unfortunately the BQ40Z50-r1 is out of stock. For this we can use this BQ40Z50RSMT IC?

    By using this any problem will occur and by uploading the golden file of BQ40z50r1 any error may occur??

  • Hello Max,

    You can use BQ40Z50 IC instead of BQ40z50-R1 IC, but before programming the golden image, the bq40z50-R1 srec must be programmed to the BQ40Z50 IC.