hi Team,
Please help us check the function of pin27, it will be low when CC is on DFP or DRP acting as DFP. Could we use this to enable or disable next stage without any SW control when the USB-C port attached a USB flash drive (DFP)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi Team,
Please help us check the function of pin27, it will be low when CC is on DFP or DRP acting as DFP. Could we use this to enable or disable next stage without any SW control when the USB-C port attached a USB flash drive (DFP)?
yes, ID is also used to control Vbus switch .
Regards
Brian
1: Make sure FP6861 is low enable.
2: vbus detect should connect to VbusB, not 5v_usb.
Regards
Brian