This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80EVM-020: BQ Studio not launching

Part Number: BQ40Z80EVM-020
Other Parts Discussed in Thread: BQ40Z80, EV2400, BQSTUDIO

Hello TI support. I have the BQ40Z80 EVM configured for a 6S pack. Between each string I have a 1kΩ resistor to act as a divider with the 6S and 7S shorted together. The “pack” is being powered off an AC wall power supply for 24V. Each string measured right around 4V. The Pres pin is tied to pack-. The jumpers are:

J16 pin22 LED

J17 pin 21 LED

J13 PDSG

J14 Pin 13 LED

J4 No jumper

J9 No jumper

J15 Pin 20 LED

J3 No jumper

J5 Pin 17 PRES

J7 Pin 12 ADC/GPIO

J8 No jumper

J10 CB7EN

J6 No jumper

J18 EV2400 SMBD1

J22 EV2400SMBC1

J11 No Jumper

 

When I apply power to the cell input, I press and hold the wake button. I can measure the pack voltage on the output while pressed to confirm that the output voltage is waking up the system. With the button held I start up BQStudio 1.3.101 but it does not recognize the device. Any ideas what needs to change in order for BQStudio to start up correctly?