Hello!
What are the upper and lower limits of the Rsns resistance that can be set for TPS2HB16?
If it is less than 1kΩ, what is the limit resistance value that can flow Isns correctly?
If it is larger than 1kΩ, what is the maximum resistance value that can be increased, except considering the effect on the MCU?
I mainly want to accurately detect a low current range of several 100mA.
Regards,