This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL497A: Boost/SEPIC converter

Part Number: TL497A
Other Parts Discussed in Thread: LM5157, LM5155

Hi Team,

A customer is looking for a non-isolated converter to boost a +12V source to +18V and -18V at the same time. The max output current is 500mA.

I find the TL497A is possible for +18V and -18V but the device only has 1 channel and they don't want to use two devices. 

I looked further but I can't find a device with 2 channels that is able to provide -18V.

Can you help further? 

Regards,

Marvin