This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5116: Device is hot

Part Number: LM5116

Hi Team,

Our customer is using LM5116 in their application but the device is hot even if the output voltage is correct. According to our customer,

I have a problem with signal form Pin LO and HO of LM5116, high side and low side MOSFET.

The yellow is LO (signal Low side) mosfet and purple is HO (High side) mosfet

Output voltage is 12V very good but IC LM5116 is so hot and buzzing sound from the inductor

I have 4 buck regulators from LM5116. 2 for 5V and 2 for 12V from 20-50V input

Attached are the schematic diagram, waveform and gerber files.

He als added,

I think the problem is in the signal on the gate G of mosfet. it's not square pulse. Can I solve this by reducing the switching frequency? Or do something to reduce the settling time of the signal.

When i connect pin 11 (DEMB) of LM5116 with resistor 10K to GND, signal in FET is square, but the IC LM5116 gets hotter when i connect it directly to ground.

Regards,

Danilo