Hi All,
I have a question about LP8866-Q1.
A customer is evaluating the LP8866-Q1.
The operating conditions are VIN=26V, VDD=3.3V, VEN=3.3V.
The customer's SCL and SDA input rise time is 350-450nsec, is this a problem?
The datasheet states that for VDD=5V, it should be within 300nsec.
Is there any information on the rise time in case of VDD=3.3V?
Best Regards,
Ishiwata