Hello, TI.
Can you please answer several questions.
1. Can you give me explanation how to properly configure SoH Load Rate to achieve adequete SoH status? I know that setting defines current that is used in SOH simulation. I have 2S battery with 3000 mAh capacity. My load is very dynamic but I assume that my average current is 6A. Should I make SoH Load Rate = 0.5 as referenced in formula in TRM? . Note that minimum value that can I write to this setting in connected battery is 0.1 and maximum is 25 for some reason.
2. Am I right that Term Voltage setting is used in capacity calculation algorithm(You call it Impedance Tracking algorithm) as lowest voltage boundary(simulates % so that when Term Voltage was reached, battery must output 0%)? And Full Discharge Voltage Thresholds(Gas Gauging -> FD -> ... Threshold) are only used for FD flag indication and doesn't affect on capacity algorithm?
Keep in touch,
Ivan