This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25703A: Does tean can help review schematic of BQ25703?

Part Number: BQ25703A
Other Parts Discussed in Thread: BQ25703

Hi team,

Can the team help review the schematic of BQ25703? 

Vin=12V

Battery pack:

3S3P 

Charging voltage:12.6V

Charging current: 2A

Cut off voltage:9V

Max discharging current:3A

another question is about the min system voltage and how to set it. 

9.5V? sys votlage will use converter boost to 18V. BQ25703 sch.pdf

  • Jimmy,

    I reviewed the schematic. Overall it looks OK. Some notes and items to fix below:

    1. I see 330uF POSCAP on VIN and VSYS, recommend to also add Ceramic caps for high frequency voltage ripple. Usually we recommend 33uF POSCAP and 4x10uF MLCC Caps + 2 DNP.

    2. Voltage divider for CELL_BATPRESZ should target 55% of VDDA for 3S, currently ~65%. Remove R454 and R457, keep R464 (100K) and R456 (64.9K) for 3S

    3. ILIM_HIZ voltage divider missing lower resistor (only see 383K pullup to VDDA), needs to be set based on planned ILIM setting:

    Regarding MinSystemVoltage: 

    - The minimum system voltage is set by REG0x0D/0C().
    - To set the minimum system voltage, write a 16-bit MinSystemVoltage register command (REG0x0D/0C()) using the data format listed in Table 27 and Table 28. The charger provides minimum system voltage range from 1.024V to 16.128 V, with 256-mV step resolution. Any write below 1.024 V or above 16.128 V is ignored. Upon POR, the MinSystemVoltage register is 3.584 V for 1 S, 6.144 V for 2 S and 9.216 V for 3 S, and 12.288 V for 4 S.

    Thanks,

    Khalid