This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS74201: TPS74201

Part Number: TPS74201


Good day,

Can you please advise, the datasheet shows that the VBias voltage can be up to 5V5 ? (Table 6.3)

However in table 6.5 it is stated to be Max 5.25V

The intent is to supply with 5v5 and have a output of 3V3. Thus connecting VBias and Vin to 5V5

Kind regards

Gerhard Ebersohn