Other Parts Discussed in Thread: TPS55288
Hi TI Teams,
Can u help to check the design of TPS55289. The schematic is show as below:

Thanks,
Kind Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Zack,
Yes, the Vin is 5 to 20V DC, the Vout is 5V, and the maximum Iout is 8A (5V/8A).
And we have another application of the TPS55289, that is, we added the I2C communication, and the input is 24V, the output voltage have 5 level (5V/9V/12V/15V/20V), and the Iout is 3A to 5A. Is there any suggestion for this application?
Thanks,
Kind Regards
Hi Lumina,
TPS55289 cannot output 5V 8A because it is out of the device current limit spec.
I would suggest you select TPS55288.
For the second application, TPS55289 could output 3A. But 20V/5A, 100W is quite challenge for TPS55289. The device thermal rise would be a concern if customer layout is not well designed.