This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
For first bring up, I must implement SMB bus for operation or it's enough to connect UVLO/OVLO and the peripheral components according to EVL that the gate FET will open and I will have 12V?
Hi Rakesh
Thanks for you help
I tried to operate the LM25066A but the FET is not open (Gate is 0), UVLO =1.5V and OVLO = 0.97V
Please help to check what I missed?
Hi Zalma,
Please remove D53 and connect the DIODE pin to GND. After doing this change please share the start-up waveforms with following signals.
VIN, VOUT, GATE, ENABLE, and TIMER