This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62086: Wrong output after a battery is drained and charged.

Part Number: TPS62086

Hi.

We are using the TPS62086 in a project we have where we need 3.3V as output. TPS62086 has as an input a 3.6V or 3.7V cell.

In rare cases when the cell is fully drained and it is charged to the minimum voltage to have 3.3V as output, for our case is between 3.35V-3.4V, we have and output of 2.1V.

Even if we charged the cell up to 4.2V, the maximum output is 2.4V, not 3.3V. Only we have 3.3V again when we disconnect and connect the cell.

Note: EN pin is connected to VIN directly and FB is connected to the VOUT through a 0Ohms jumper resistor. 

So, could you tell us why this is happening and how we can solve this issue?

Regards.