This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS74901: TPS74901: When input=3.3V and output 1.8V, how to configure Vbias?

Part Number: TPS74901


Hi team,

As we know that the VBias must be 1.75V above Vout.

In this case, Vbias need at least > 3.35V(1.8V+1.75V = 3.35V). but the board doesn't have 5V source.

Could we use resisters to divide 12V source to 5V for VBias? If not, do you have any suggestions for this application?

BR,

Jimmy

  • Hi Jimmy,

    Using a resistor divider could work, but the output voltage can be unreliable unless the resistors are sized to have at least 10mA through them or more, given the BIAS pin current of 1mA (typ) or 2mA (max). A more robust and accurate way to do it would be to either use another regulator for it, or use a shunt voltage reference. 

    Regards,

    Nick