Hi guy i have some question on this device TPS63030DSKR i do the 2 typical designgive in the datasheet but i dont have the 3.3V in aouting
i use for R1 R2 this 2 value 840K and 150K i can have some help please ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi guy i have some question on this device TPS63030DSKR i do the 2 typical designgive in the datasheet but i dont have the 3.3V in aouting
i use for R1 R2 this 2 value 840K and 150K i can have some help please ?
yes i have one question dissipation pad is connect at gnd ? and the pin 9 and 3 is aslo connect at gnd and dissipation pad ?
i change the value of r2 r1 for 200k and 1120k and vout = vin on oscilloscope
Hi Jeanmarc,
yes, that is correct, you can connect the EHP and PIN 3,9 together to GND.
Regards
Tao