This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80: Custom Firmware

Part Number: BQ40Z80

Hi,

Good Day. The customer had seen that the chip has an integrated MCU which has an integrated flash. That flash can be reprogrammed. But can you tell us if the firmware that is running on this chip can be replaced with a custom one or if just TI can provide compatible firmware?

Please advise. Thank you very much.

Best Regards,

Ray Vincent

  • Hello Ray,

    If there is a requirement that would add value, then TI has the capability to customize the firmware for a specific application.

    You can DM me so that we can get into the details of the requirement and i can loop in others as required.