Hi,
I will use TPS62136 for 5G Module.
 In the example power diagram in the 5G Module HW Design Guide, it is recommended to use 2 x 220uF capacitors at the module input.
Reference circuit:
https://drive.google.com/file/d/1CRF08FVHV61a5waHIUr0RnXt7wvWT8UJ/view?usp=sharing
Question 1: If I connect two 200uF Tantalum and ESR 0.4 OHM capacitors to the output of TPS62136 as suggested here, will I have a problem?
Question 2: I have stock of the 470uF 6.3V 0.4 OHM ESR tantalum capacitor in the link below. If I use 2 x 470uF instead of 2 x 220uF, will I have problems and what should I pay attention to?
I have used 2 x 470 uF in a different regulator before and the possibility of instability in this case was written to me in the last post here. By the way, I solved my problem here, the problem was caused by the production of the capacitors I used.
e2e.ti.com/.../tps62086-explosion-of-the-tantalum-capacitor-connected-to-the- tps62086-output
Regulator input will be 5V 3A adapter. I am looking for the best and smoothest combination I can create with the TPS62136 for a 5G module powered by 3.7V, which may have high current consumption and peak currents.
Thanks.