Dear Support,
We have observed that when more voltage beyond absolute maximum of 7V is given to TPS54116-Q1 IC. Input is getting shorted to output SW pins and it is damaging the output power connected circuits. We wanted to have protection in such a way that any over voltage should only damage IC but it should not short the input voltage to output. Let us know the solution.
Regards,
Erfan