This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55288: Is I2C input required while using TPS55288

Part Number: TPS55288


Hi,

I want to design simple solar battery charger without microcontroller.

Is TPS55288 is suitable for such application. (Non-isolated, 8V to 24V input; 13.5V output @ 3A current)

It has I2C communication, I don't need it. Can I leave those pins floating.

Or can you please suggest any other PWM IC for such application?

Regards,

Abhishek D.