Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1146: USB VESA spec

Part Number: TUSB1146

Hi team,

what's the definition of this 8.5dB at host device?

for example,

if the total PCB loss is 20dB, and our redriver can compensate 12dB, which means we still have 8dB loss left which is within the USB host spec (8dB<8.5dB).

so it means we're still within the spec and can pass the compliance  , right?

Regards,

Fred