This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I want to evaluate a dual phase Buck Converter done with TPS62480 against a Discrete N-MOS H-D Buck.
The Design of the Discrete Buck is the following :
Vin = 3.7V,
PWM = 0-3.3V, 100kHz, duty-cycle ~0.5
The design has been done by a fellow engineer so I don't fully understand it. Especially the use of a NMOS for the High-Drive side and the supposedly "bootstrap" to drive it.
From my calculation, the inductor seems to be too low, causing current ripples of about 0.9 A. Can someone confirm if this circuit can perform as a Buck ?
Hi Alex,
It's not clear what you need. I suggest talking to whoever drew that circuit to understand the purpose of it.
Instead of the older TPS62480, we have single phase devices that offer higher efficiency and smaller size, such as TPS62867.
Thanks,
Chris