Part Number: LM2671
Other Parts Discussed in Thread: LM2675
Hi Experts,
Good day. Seeking your assistance on these clarifications with buck converters:
We are having availability issues with the LM2671-5.0/NOPB but the design (pcb layout) also allows for the feedback resistors for the LM2671-ADJ/NOPB part. Unfortunately, we are also experiencing availability issues with this. Questions are:
1) Is it possible to use LM2671-3.3/NOPB with a 3K6 feedback resistor to give 5.0V ?
2) Is it possible to use LM2675-5.0/NOPB without changing the inductor (we still only need 500mA output) ?
2a) Is it possible to use LM2675-3.3/NOPB with feedback resistor ? (as 1)
3) Is it possible to use LM2675-ADJ/NOPB ( comment as for (2) ) ?
My concerns with using a feedback resistor are that the data sheet may not be telling the whole story in respect of FB pin
impedance and availability on fixed voltage devices, and possible impact on stability. We can tolerate increased Vout up to 5.5V.
For your assistance please.
Regards,
Archie A.