This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL783: Output drop

Part Number: TL783


Hi team,

We have trouble about TL783 circuit.

When the power is turned on, it regulates to 24V, but after few minute the output gradually drops to about 17V.

-We use Cadj, could this be the cause?

-We are using 1kΩ for R1, but if the load current is 15mA or more, will it work even if it is not 82Ω?

-A large value of R1 increases the effect of leakage from the ADJ pin. Could this be the cause?

Best Regards,