This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25730: Solution for Power path management on USB and AA battery ×2

Guru 19655 points
Part Number: BQ25730
Other Parts Discussed in Thread: BQ25620

I looking for the solution about USB (5V) and AA battery ×2 (2~3V) with Power path management.

(When system load higher than I_BAT or I_USB, the other side provide current fill in the gap)

Can bq25730 or the other bq257xx series make above solution?

・If yes, are there any reference design or application note?

・If no, is there any matched IC?

※AA battery chemistry are both case of NiMH, Alkaline, and Lithium.

Best regards,

Satoshi