Other Parts Discussed in Thread: BQ25060, , BQ51013B
Hello TI forums.
We are using the BQ51013A Qi wirelss power supply receiver IC combined with a BQ25060 Li-ion battery charger IC, as per the following diagram (PDF). We have designed for a 1.0A charging current, but we are only seeing 500mA at the battery.
The Li-ion battery is represented by connector J2. It is a 1S2P 3.7V Li-ion battery pack (two 18650 cells in parallel with integrated BMS with 10k thermistor)
We desire to charge the battery with IOUT = 1.0A. As such, we have made the following design choices:
- BQ25060:
- EN pin pulled down to ground,
- ISET pin pulled to ground via 1k resistor (R5)
- BQ51013A:
- ILIM pin linked to ground via total "RILIM" resistance of 110R + 140R (R4 and R2, respectively) = 250R total. This should set IMAX to 1.0A.
- We have followed the standard process of measuring the inductance of the RX coil in--situ in the device to derive the correct resonant capacitor values.
Using an Otii Arc battery simulator, I record the current arriving at the battery as follows:

In the above graph, the Y-axis is current in mA, X-axis is time in seconds. Negative current means current entering the battery, ie. charging. The spikes show that the rest of the circuit is drawing current during the charging process occasionally). On average the battery receives 500mA, which is half of the desired charging current of 1000mA.
The Qi transmitter we are using is an off-the-shelf charging pad that should be capable of delivering 10W output. We have tried multiple different charging pads, but we are experiencing the same charging current across all of them.
Please could you review our circuit diagram, to see if we have made any mistakes in our design? Or are there any other factors we have missed and could change to achieve 1.0A charging current?
With kind regards,
Aran