Other Parts Discussed in Thread: BQSTUDIO, GPCRB
Hello,
I'm having some doubts about the Chemistry Programming.
We're using the Panasonic NCR18650B battery. This one:
But everywhere on the internet it says it's 3400mAh. AliExpress for example:
And it's not only AliExpress. It's everywhere: 3400mAh.
But on bqStudio, these are the options for Panasonic NCR18650B:
Both say 3350mAh. In fact, there is no NCR option for 3400mAh. And it's such a common battery.
So, my questions are:
1) What should I do (besides Chemistry ID Matching)? Simply use the option I highlighted on the image above?
2) Is there a common 18650 battery that I can easily buy that's already listed on bqStudio, so that I don't need to perform the Chemistry ID Matching? We did attempt this a few times but it probably requires a level of precision that we're not able to get.
Thanks in advance!