Other Parts Discussed in Thread: BQSTUDIO, , EV2400
Hello
I respect that EV2300 is obsolete but I have one and the release notes for BQStudio reference EV2300 changes so I'd like to try to use it with BQ76592.
If I confirm that it now works (for I2C), I can give an update to Matt Sunna feedback here:
My question is how I enable the VOUT on the I2C port on EV2300 to provide 5V. I want to use it as the I2C bus pull-up voltage.
VOUT is switched by Q2 which is enabled when the EV2300 MCU RA4 pin is driven low. There is no additional jumper so some soft command is necessary.
I cannot see any configuration in BQStudio so I may have to adjust it "independently" with some USB commanding.
Thank you
Harry