Hi
The customer design with BQ25601, After the battery is over discharged, the battery voltage is 0V, and the external charger cannot be charged.
The log data from system read 4.2V (the system ADC reads the voltage at Vbattery), but the actual battery voltage is 0V.
The chip is BQ25601, Attached the schematic the chip name is incorrect, it is BQ25601's schematic.
Attached the system log data
Why the battery voltage is 0V, but the system reads 4.2V?
Thanks
Star