Team,
Looking at 7.4.8 FAULT RECOVERY in the datasheet, the recovery condition is EN = HIGH and the brightness is greater than zero. If EN is HIGH but brightness is zero, does the device keep the state FAULT recovery?
Regards,
Saito
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Team,
Looking at 7.4.8 FAULT RECOVERY in the datasheet, the recovery condition is EN = HIGH and the brightness is greater than zero. If EN is HIGH but brightness is zero, does the device keep the state FAULT recovery?
Regards,
Saito
Hi, Saito-san
I think you can combine the Table 7-9 together with the FAULT RECOVERY.
When you enter the FAULT RECOVERY, mostly device has a brightness to lead the fault
Hi Zhiqian-san,
I understand the mostly device has a brightness when the device enter the FAULT RECOVERY state. But, when the device enters the FAULT RECOVERY state, and then we set EN=HIGH and set brightness to zero, does the device keep the state FAULR RECOVERY?
Regards,
Saito
Hi, Saito-san
You can follow the Table7-9 to see the specific action for different fault.
Some will be in standby mode, some will recover after 100ms.