Other Parts Discussed in Thread: BQ24179, BQ25792, BQ25798, BQ25720
Hello,
I would like to incorporate the BQ25790 battery charging IC in a new design, and I have some questions as follows:
The battery I would like to charge is an Ni2020HD29 which is a 94 watt-hour 10.8V 3S 3P smart bus device. Should the BQ25790 be capable of accommodating this battery?
The design will have a processor which will use I2C bus to interrogate the battery status. Can I do this just using the I2C clock and data lines, and let the BQ25790 perform its charging autonomously?
If the BQ25790 becomes unavailable, can the BQ24179 be used in its place?
I will need to limit the max charging current to 4A. Is this a relatively simple thing to do?
The device may be in storage for a long time with the charging source removed, and the processor powered down. Would you advise using ship mode / shutdown to conserve battery power? Can the BQ25790 be easily restarted when the processor is restarted?
Another device I am interested in using is the BQ25792. Would this be suitable, and is there is similar (identical pinout) device that I could use if this became unavailable?
Best regards
Martin Lindsay
Ocean Technical Systems