This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5002: High side switch for

Part Number: LM5002
Other Parts Discussed in Thread: LM5022, LM5121

Hello Team,

                    I have a boost circuit using LM5002 as shown

I want to put a switching mechanism on the high side, i.e the left of the circuit. This circuit is used in a BMS as a BOOST to charge the battery.

Would High side switching or Low side switching be better for 48V and 4-6 A.

The switch should be controlled by the onboard Microcontroller.

Could you kindly recommend any switching mechanism to achieve this.

If possible could you kindly provide a reference design or anything to help me out 

Thanks