This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54200: Description of shutdown-and-latch mode protection and auto-retry mode protection

Part Number: TPS54200
Other Parts Discussed in Thread: TPS54201

Hi Team,

I am promoting TPS54200/TPS54201 and noticed that there are 2 different modes, but I did not find description.

Could you help to describe or share some materials of these 2 modes?

Thanks,

Rebecca

  • hello Rebecca

    I am working on this, will feedback to you when I have some results.thanks

  • Hello Rebecca

    for shut down and latch mode, once the fault is triggered, the device enters shutdown mode and FET keeps off. The only way to activate the device is to re- power  input voltage, otherwise it stays in shut down.

    for auto-retry mode, once the fault is triggered, device enters shutdown mode, but if current or voltage comes back to normal value, the device can work again and there is no need to re-power input voltage.