Hi
I have designed a DC/DC buck converter using UCC27211D (package without thermal pad die) and it works great. Now the problem is that the UCC27211D is out of stock and I find that the UCC27211DDA have the same pinout but with a thermal pad die. I wonder if I can use the UCC27211DDA in the same PCB without connecting thermal PAD die or I'm obliged to make a new PCB adapted to the UCC27211DDA
Thank you