Part Number: TPS631000
Other Parts Discussed in Thread: TPS630242
Hi,
In the below section of TPS631000 datasheet.

It saying Current can flow from output to input. It seems if the Vout>Vin then the flow of output current to input can cause voltage rise on the input terminal right? I afraid this can cause leakage problems. Suppose my input is 2.7V and output 3.3V. leakage from output will cause rise in the input supply right? can you clarify?