This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65132: evaluate a 10uF/0402/10V capacitor for the REG pin

Part Number: TPS65132


Hi team,

There are some questions in TPS65132 design to consult you.

Since the project does not reserve another capacitor position, the risk of a 0402 capacitor needs to be evaluated.

1. What is the effective capacitance requirement for the REG pin circuit at operating voltage?
2. At present, only a capacitor of 10uF/0402/10V is attached to the circuit, does it meet the requirements of the IC?
3. If the effective tolerance values of the pins at this point are not met, what effect will this have on the load?

Thanks 

Best regards 

Lillian