Part Number: TPS63070
Other Parts Discussed in Thread: TPS54201
Hi,
Reading the Driving a Peltier Element (TEC): Efficiency and Aging left me with a question.
My intend is indeed to use a constant current source, and I do want the ability to control the TEC in both directions. So a boost-buck converter seems to be the best solution.
However, in my application accurate temperature control is not necessary. The device should either be cooled or warmed as much as possible in a short period of time (seconds).
Most of the buck-boost converters (which are not very new or expensive) do not come with a large input/output voltage difference. The TEC is current controlled but the total Watt will still determine the amount of cooling or heating of the device.
The TPS63070 can have a potential difference of 16-2.5=13.5[V]. Would this not be easier to create and control with for example the TPS54201 and the circuits as James suggested in:
Best regards,