Hello,
The problem is that the module squeaks and whines when it works.Please help to analyze where the squeaks and whines come from.Thanks!
--chen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
The problem is that the module squeaks and whines when it works.Please help to analyze where the squeaks and whines come from.Thanks!
--chen
Hi Chen,
We have numerous copies of this EVM here and they do not make any squeaks or whines, or other audible noise.
Thanks,
Stephen
the voltages on IN:
the voltages on OUT:
the voltages on EN:
the voltages on BIAS:
Hi Chen,
Can you place these measurements on the same oscilloscope plot?
Can you zoom in to one of the sets of noise? We need to see if we can identify what is happening first, noise on VIN or noise on VOUT.
It looks like you have 5V on the input and 1V on the output - can you confirm? What is your load current during these tests?
Can you try a different bench supply powering VIN and VBIAS? The repetition rate of the dirty waveforms looks to be around 50-60 Hz, so perhaps the power supply has an issue.
Thanks,
Stephen