This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54331: TPS54331 OC Issue

Part Number: TPS54331
Other Parts Discussed in Thread: TPS54531

Dear Team,

Customer use TPS54331DR in their Thermal Printer,Vin 12V,Vout 8.5V.

When they do all balck print test (Load current is 5-6A),the total amount is 80PCS,then found the output voltage of  device is drop 5.5V(about 4PCS) and other output voltage is 7V(76PCS).7V can Make the print module work and 5.5V can not make the print moudle work.

I think the TPS54331DR is over current protect and 5.5V/7V is the difference of different device caused.Pls help to confirm.

BTW,pls kindly find the attach file for OS test data and schematic.

Thanks54331 OS Test Data.xlsx