This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74722-Q1: Ideal Diode as High side power rail controller

Part Number: LM74722-Q1
Other Parts Discussed in Thread: BQ34Z100-G1, LM5060-Q1

Hello Team,

                   We are designing a BMS around the BQ34Z100-G1. The battery specs are max 54.6V and 6A. We want to implement a high side switch for the power rails and it would need to be controlled by the GPIO of a Microcontroller. We wanted to know if we can use LM74722-Q1 as a high side switch where the power will flow through the path by enabling the LM74722. 

If this is not suitable could kindly recommend which TI product will help us in this regard 

Thanks