This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54331: Under Volt Lockout problem.

Part Number: TPS54331

Hello,

I have designed buck power supply using TPS54331. It is converting the voltage as it have top be.  Also. I have used a divider at EN for UVLO for 11 Volt. Now the circuit turns on at 11V but when I reduced the voltage below 11 it is not shutting down instead it is shutting down at around 10.2V, any ideas on that?