Hi team,
Customer has some questions
The device with UCC27324D model has a power supply voltage range of 4.5-15V. When testing VOH, 10mA is required. When the power supply voltage is 4.5V, the VOH value is lower than the lower limit. When the power supply voltage is 15V, 10mA is used to test that the VOH value is normal. Is this abnormal? Under 4.5V power supply during factory test, does the VOH index with 10mA load meet the manual requirements?
Could you help?
Thanks & Regards,
Jiahui