Other Parts Discussed in Thread: USB-PD-CHG-EVM-01
Hello,
I am having charging issues with my system. I have a tablet connected to USB-PD-CHG-EVM-01 to source power into tablet.
I have these configurations with the GUI Software tool (version 7.04)
When I program the USB-PD-CHG-EVM-01 with the configurations from the screenshot above, I can only source 700mA.
When I connect my USB wall charger directly to the tablet, the tablet consumes 1.7A at 5V.
I am using the same tablet for both tests. I am not sure why the TPS negotiates less power than if i connect directly to the wall charger.
I would like to source as much current to the tablet as possible for fast charging.
Please advise.
Thanks,
Victor