Hi team,
Could you please help advise -
- What is the softstart reference voltage? 0.8V? Customer need to measure the softstart time at SS pin.
- What is the switching frequency during softstart and how does it change?
- "A failsafe current limit set at 1.2 A, or 1.6 times the nominal peak current limit, provides redundant fault protection in case of transformer short circuit or saturation effects." ==> how can customer test the 1.2A current limit? The current test result shows current limit at 0.75A.
- In datasheet, there are VCC wordings in page 12 and page 15 - are they just typo and should be BIAS?
- How to test UVLO threshold for BIAS?
- Thermal shutdown - is there any waveform or test result on thermal shutdown?
- What is shutdown level at EN/UVLO pin? 1.1V or 0.6V? There are multiple places stating this threshold in datasheet, some are 1.1V and some are 0.6V.