This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-DEVICE-FW: R4: Voltage-Based Balancing when Relaxed not working

Part Number: BQ40Z50-DEVICE-FW

Hi

We are trying out the Voltgae-Based Balancing for our 4S1P LFP battery, since the normal balancing algorithm was unbalancing our cells, rather than balacing.

The voltage-based balancing during charging seems to work, but the balacing during rest doesn't seem to be triggered. [BCR = 1] is enabled and we also disabled [LFP_Relax = 0] in order not to have to wait for 2 days. Also, BCR was working when we had the old balancing algorithm in R2 active:

Could it be that BCR doesn't work at all with Voltage-Based balancing because the increased thresholds (caused by the window logic) would need to be reset constantly, but in the TRM it only says:

"The cell balance threshold is reset to the value in Voltage Cell Balance Threshold at the start of every charge and reset cycle." (I don't really understand, what "reset cycle" means though).

Thanks in advance for your help,

Mark