This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3485: Alternate P-FET in SOT-23-6 package

Part Number: LM3485


Buck regulator team,

I could use some help finding a good replacement P-FET to use with the LM3485.  Webench recommends the FDC5614P in a SOT-23-6 package, which the customer used.  This is very difficult to source right now, so we're looking for alternates in the same package. 

Vin is 20 to 28V

Vout is 3.3V at 0.5A

I found these ones with similar or better RDSon.

Diodes Inc DMP3056LDM-7

Diodes Inc ZXMP3A17E6TA

On Semi CPH6341-TL-W

Can you help confirm for me if they would be good choices for this application?

Thanks,
Darren